IMPORTANT: This step is required only if you are using Internet Explorer to access the APM Connect Administration Center. If you are not using Internet Explorer, you can skip this procedure, and proceed to the next step, in the APM Connect Base First-Time Deployment Workflow.
Steps
On the APM Connect server, access Control Panel\Network and Internet, and then select Internet Options.
The Internet Properties screen appears
The Security Settings -Intranet Zone screen appears.
In the Settings section, access the Include local directory path when uploading files to a server, and select Disable.
Select OK.
The Security Settings -Intranet Zone screen closes.
Internet Explorer is configured accommodate APM Connect.
What's Next?
Copyright © 2018 General Electric Company. All rights reserved.